Interpolation data record (position set-point)
Index.Sub | 60C1.1H |
Data Type | Integer32 |
Access | Read/Write |
PDO Mappable | RX_PDO (1) |
Unit | User-defined position unit (2) |
Range |
-2147483648 to 2147483647 |
Default Value | -- |
Store Supported | No |
Description |
This object defines the position set-point used for linear interpolation used for Interpolated Position Mode (ip). |
Notes |
(1) available with firmware V00r74 or superior. (2) See Factor Group. |